Using Timer INT without Hardware Pin-Out MATx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Timer INT without Hardware Pin-Out MATx

669 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by StephenHawkings on Mon Sep 12 02:34:49 MST 2011
Dear Collegues,
would wou agree that it's possible to use the timer INTs without changing the corresponding I/O pins (MATx and CAPx)? I just want to use the timer interrupts internal, but keep the I/O pins as simple I/Os. (I use LPC1114, but probably behaviour is the same across all LPCs.)

Thank you for your comments!
StephenHawkings
0 Kudos
Reply
1 Reply

662 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Sep 12 02:38:08 MST 2011
In general....yes :)
0 Kudos
Reply