Using Link with LPC 810

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Link with LPC 810

6,771件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Tue Dec 23 08:41:46 MST 2014
Hi, everyone.
I have a LPC Expresso 1769 Board. And I planning to buy some LPC810.
And I tried to find some info about using LPC-Link of 1769 Board with LPC810.
Its possible without cutting the board? And where can I find how to connect the boards?

Thanks
Daniel
0 件の賞賛
返信
9 返答(返信)

6,752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Dec 26 11:16:35 MST 2014

Quote: Mega
But the other  3 pins doesnt need resistor? Im just asking because of the 3rd image content



GND doesn't need a pull-up  :bigsmile:

Pulling-up / down for SWDIO and SWCLK isn't required...
0 件の賞賛
返信

6,752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Fri Dec 26 11:02:44 MST 2014
But the other  3 pins doesnt need resistor? Im just asking because of the 3rd image content

Thanks
0 件の賞賛
返信

6,752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Wed Dec 24 02:47:57 MST 2014
Thanks a lot =) Now my mind is clear


Quote: R2D2

Quote: Mega
So the "only" think I need to worry about is to correspond the pins of this images.



SWD is working with a simple 4-wire connection:

SWDIO, SWCLK, Reset and GND. Some parts don't use Reset, but I'm not sure if LPC8xx is using it.

Connect them from J4 to your target chip and disconnect (cut) them from the LPCXpresso target board (LPC1769).
Otherwise LPC-link is seeing 2 targets  :(( 

Then add a pull-up (10k) to Reset and connect 3.3V to your target  :)

That's all  :O


0 件の賞賛
返信

6,752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Dec 23 21:16:21 MST 2014

Quote: Mega
So the "only" think I need to worry about is to correspond the pins of this images.



SWD is working with a simple 4-wire connection:

SWDIO, SWCLK, Reset and GND. Some parts don't use Reset, but I'm not sure if LPC8xx is using it.

Connect them from J4 to your target chip and disconnect (cut) them from the LPCXpresso target board (LPC1769).
Otherwise LPC-link is seeing 2 targets  :(( 

Then add a pull-up (10k) to Reset and connect 3.3V to your target  :)

That's all  :O

0 件の賞賛
返信

6,751件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Tue Dec 23 20:38:58 MST 2014
My bad, sorry, I read all again. I has a bit confusing about pinning

So the "only" think I need to worry about is to correspond the pins of this images. And apply some resistors. On LpcExpresso IDE do I need change something?
I think I will buy the 810 tomorrow.

And where should I conect JTAG RTCK?

[[img]http://www.lpcware.com/system/files/pinning1.jpg[/img]
[img]http://www.lpcware.com/system/files/pinning2.jpg[/img]
[img]http://www.lpcware.com/system/files/pinning3.jpg[/img]
Thanks for all help and patience
0 件の賞賛
返信

6,751件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Dec 23 20:13:43 MST 2014

Quote: Mega
But I need LPC800 Mini-Kit?



For what? As target?
0 件の賞賛
返信

6,751件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Tue Dec 23 19:49:29 MST 2014
But I need LPC800 Mini-Kit?
0 件の賞賛
返信

6,751件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mega on Tue Dec 23 19:22:16 MST 2014
I was missing this http://www.lpcware.com/content/faq/lpcxpresso/debug-design
Thanks =)
0 件の賞賛
返信

6,751件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Dec 23 09:17:23 MST 2014

Quote: Mega
Its possible without cutting the board?



Yes, it's important to cut the SWD connection, not the board...

http://www.lpcware.com/LPCXpressoV1Boards


Quote: Mega
And where can I find how to connect the boards?



Forum search:

http://www.lpcware.com/content/faq/lpcxpresso/debug-design

http://www.lpcware.com/content/forum/using-lpc810-board-with-lpc-link


0 件の賞賛
返信