Using LPCXpresso without a LPC card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using LPCXpresso without a LPC card

774件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by boudriga.habib on Tue Jul 19 06:00:49 MST 2011
Hello
I'm novice in embeded programming and i have just downloaded the LPCXpresso i wanted to ask you if i can use this IDE without having a physicaly card liated to my computer. Maybe there is kind of software solution

Thank you
0 件の賞賛
返信
1 返信

765件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jul 19 09:04:00 MST 2011
The LPCXPresso IDE does not provide any form of software simulator - you have to use it with real target hardware - either an LPCXpresso board, a Code Red RDB1768 board or a supported MCU on a board which you connect to using the LPC-Link portion of the LPCXpresso board, or using Code Red' Red Probe+ product.

Regards,
CodeRedSupport
0 件の賞賛
返信