Using Flash as permanant Data storage memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Flash as permanant Data storage memory

719 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Mon Jan 23 05:32:44 MST 2012
I am using LPC1769, for one of my project I need to store data permanently. Can I use on chip flash for the same purpose?
If it is possible how to do it?:confused:
0 Kudos
Reply
1 Reply

704 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Skashkash on Mon Jan 23 08:40:58 MST 2012

Quote: Sharadanand
I am using LPC1769, for one of my project I need to store data permanently. Can I use on chip flash for the same purpose?
If it is possible how to do it?:confused:



You can use the the IAP commands to copy data to flash.
Check the UM section 32.8 IAP commands.
0 Kudos
Reply