Using Flash as permanant Data storage memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Flash as permanant Data storage memory

682件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Mon Jan 23 05:32:44 MST 2012
I am using LPC1769, for one of my project I need to store data permanently. Can I use on chip flash for the same purpose?
If it is possible how to do it?:confused:
0 件の賞賛
返信
1 返信

667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Skashkash on Mon Jan 23 08:40:58 MST 2012

Quote: Sharadanand
I am using LPC1769, for one of my project I need to store data permanently. Can I use on chip flash for the same purpose?
If it is possible how to do it?:confused:



You can use the the IAP commands to copy data to flash.
Check the UM section 32.8 IAP commands.
0 件の賞賛
返信