Using Code Red with Olimex and other boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Code Red with Olimex and other boards

935件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pauljurczak on Wed Mar 23 00:10:31 MST 2011
Hi,

I'm trying to choose ARM Cortex development environment and I would like to know, if there are any problems with using Code Red tools with Olimex and other boards. I'm OK with having to use LPC-Link, if necessary, but I don't want to be restricted to LPCXpresso boards only.

Thank you,
Paul
0 件の賞賛
返信
2 返答(返信)

925件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Mar 23 04:34:53 MST 2011
These links might give you some hints on splitting the LPC-Link from the MCU portion of the LPCXpresso board so that you can use it with your own custom or purchased board:

http://knowledgebase.nxp.com/showthread.php?t=1653

http://knowledgebase.nxp.com/showthread.php?t=52

http://verhoeven272.nl/fruttenboel/ARM/EAxpres1343.html

HTH!
0 件の賞賛
返信

925件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 23 00:35:17 MST 2011
Just connect SWD & Reset and you can use every board you want. I'm doing that since 2009 with all my own boards without problems.

SWD:

http://support.code-red-tech.com/CodeRedWiki/CM3_SWD
0 件の賞賛
返信