Using CMSIS with LPC1114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CMSIS with LPC1114

916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tcrussell on Thu Jan 07 17:12:50 MST 2010
The system clocks get set in the CMSISv1p30 project in the system_LPC11xx.c file.  What is the proper way to make changes to the clock settings or enable/disable the PLL?  Should I modify this source?  At the top of the file it says "Use configuration wizard in context menu", but I don't see this in LPCXpresso.

Tom
0 件の賞賛
返信
1 返信

882件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Jan 08 02:04:31 MST 2010
Yes, you can edit the file.

The comments relate to Keil uVision.
0 件の賞賛
返信