Using CMSIS with LPC1114

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CMSIS with LPC1114

920 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tcrussell on Thu Jan 07 17:12:50 MST 2010
The system clocks get set in the CMSISv1p30 project in the system_LPC11xx.c file.  What is the proper way to make changes to the clock settings or enable/disable the PLL?  Should I modify this source?  At the top of the file it says "Use configuration wizard in context menu", but I don't see this in LPCXpresso.

Tom
0 Kudos
Reply
1 Reply

886 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Jan 08 02:04:31 MST 2010
Yes, you can edit the file.

The comments relate to Keil uVision.
0 Kudos
Reply