User App does not work...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

User App does not work...

552件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alanisgp on Wed Mar 07 06:04:32 MST 2012
Hi, I have successfully managed to run the application, in fact, download the binary image and burn it to flash. The problem I have found then is that it hangs when trying to run the user application. I followed all the steps to create the corresponding script link to the binary image.
Why not run?. The question that arises if the initialized data from the user application are copied from flash to RAM, as this is done by ResetISR (), which, from the point of view of the execution of the secondary bootloader is never invoked in the user application as a reset is not effected due to routing is performed by a jump of code.??? Any suggestions?
Thank you very much and best regards
0 件の賞賛
返信
0 返答(返信)