Unused variables in LPCOpen library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused variables in LPCOpen library

1,552件の閲覧回数
hmyoong
Contributor III

lpc_chip_43xx/src/spi_43xx.c

/* Clean all data in RX FIFO of SPI */
void Chip_SPI_Int_FlushData(LPC_SPI_T *pSPI)
{
volatile uint32_t tmp; // <----- Not used
Chip_SPI_GetStatus(pSPI);
tmp = Chip_SPI_ReceiveFrame(pSPI);
Chip_SPI_Int_ClearStatus(pSPI, SPI_INT_SPIF);
}

lpc_chip_43xx/src/uart_18xx_43xx.c

/* Initializes the pUART peripheral */
void Chip_UART_Init(LPC_USART_T *pUART)
{
volatile uint32_t tmp; // <----- Not used

/* Enable UART clocking. UART base clock(s) must already be enabled */
Chip_Clock_EnableOpts(UART_PClock[Chip_UART_GetIndex(pUART)], true, true, 1);

/* Enable FIFOs by default, reset them */
Chip_UART_SetupFIFOS(pUART, (UART_FCR_FIFO_EN | UART_FCR_RX_RS | UART_FCR_TX_RS));

//...

}

ラベル(2)
タグ(1)
3 返答(返信)

1,283件の閲覧回数
adamrakam
Contributor III

/* Clean all data in RX FIFO of SPI */
void Chip_SPI_Int_FlushData(LPC_SPI_T *pSPI)
{
volatile uint32_t tmp;
Chip_SPI_GetStatus(pSPI);
tmp = Chip_SPI_ReceiveFrame(pSPI);  // <----- used here
Chip_SPI_Int_ClearStatus(pSPI, SPI_INT_SPIF);
}

I would expect it has sth to do with a compiler/an optimization but I might be completely wrong.

1,283件の閲覧回数
hmyoong
Contributor III

I did not look down of the lines. You are right, the default optimization removes it. Need to dissambly the code to see the differences.

1,283件の閲覧回数
adamrakam
Contributor III

You are right, the default optimization removes it.

Removes what ?

This is how "Chip_SPI_ReceiveFrame()" is defined :

STATIC INLINE uint16_t Chip_SPI_ReceiveFrame(LPC_SPI_T *pSPI)
{
    return SPI_DR_DATA(pSPI->DR);
}

I suppose :

The volatile keyword is used to force a compiler to call the function "Chip_SPI_ReceiveFrame()". If the variable tmp was defined without volatile keyword i.e. just "uint32_t tmp", calling of the "Chip_SPI_ReceiveFrame()" would not be guaranteed. In this case a compiler might think: "hm, return value from "Chip_SPI_ReceiveFrame()" is stored in the non-volatile "tmp" variable on the stack and "tmp" is not used till the end of the "Chip_SPI_Int_FlushData()" so i will not call(inline) it and save time/memory."

But the volatile keyword does not give a compiler any chance to be ambiguous about calling "Chip_SPI_ReceiveFrame()"  - keyword volatile guarantees that calling "Chip_SPI_ReceiveFrame()" will not be optimized away.