Unused variables in LPCOpen library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unused variables in LPCOpen library

1,547 次查看
hmyoong
Contributor III

lpc_chip_43xx/src/spi_43xx.c

/* Clean all data in RX FIFO of SPI */
void Chip_SPI_Int_FlushData(LPC_SPI_T *pSPI)
{
volatile uint32_t tmp; // <----- Not used
Chip_SPI_GetStatus(pSPI);
tmp = Chip_SPI_ReceiveFrame(pSPI);
Chip_SPI_Int_ClearStatus(pSPI, SPI_INT_SPIF);
}

lpc_chip_43xx/src/uart_18xx_43xx.c

/* Initializes the pUART peripheral */
void Chip_UART_Init(LPC_USART_T *pUART)
{
volatile uint32_t tmp; // <----- Not used

/* Enable UART clocking. UART base clock(s) must already be enabled */
Chip_Clock_EnableOpts(UART_PClock[Chip_UART_GetIndex(pUART)], true, true, 1);

/* Enable FIFOs by default, reset them */
Chip_UART_SetupFIFOS(pUART, (UART_FCR_FIFO_EN | UART_FCR_RX_RS | UART_FCR_TX_RS));

//...

}

标签 (2)
标记 (1)
3 回复数

1,278 次查看
adamrakam
Contributor III

/* Clean all data in RX FIFO of SPI */
void Chip_SPI_Int_FlushData(LPC_SPI_T *pSPI)
{
volatile uint32_t tmp;
Chip_SPI_GetStatus(pSPI);
tmp = Chip_SPI_ReceiveFrame(pSPI);  // <----- used here
Chip_SPI_Int_ClearStatus(pSPI, SPI_INT_SPIF);
}

I would expect it has sth to do with a compiler/an optimization but I might be completely wrong.

1,278 次查看
hmyoong
Contributor III

I did not look down of the lines. You are right, the default optimization removes it. Need to dissambly the code to see the differences.

1,278 次查看
adamrakam
Contributor III

You are right, the default optimization removes it.

Removes what ?

This is how "Chip_SPI_ReceiveFrame()" is defined :

STATIC INLINE uint16_t Chip_SPI_ReceiveFrame(LPC_SPI_T *pSPI)
{
    return SPI_DR_DATA(pSPI->DR);
}

I suppose :

The volatile keyword is used to force a compiler to call the function "Chip_SPI_ReceiveFrame()". If the variable tmp was defined without volatile keyword i.e. just "uint32_t tmp", calling of the "Chip_SPI_ReceiveFrame()" would not be guaranteed. In this case a compiler might think: "hm, return value from "Chip_SPI_ReceiveFrame()" is stored in the non-volatile "tmp" variable on the stack and "tmp" is not used till the end of the "Chip_SPI_Int_FlushData()" so i will not call(inline) it and save time/memory."

But the volatile keyword does not give a compiler any chance to be ambiguous about calling "Chip_SPI_ReceiveFrame()"  - keyword volatile guarantees that calling "Chip_SPI_ReceiveFrame()" will not be optimized away.