Unsure how to enable UART interrupt.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unsure how to enable UART interrupt.

827件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mngeowcy on Fri Apr 10 06:56:17 MST 2015
Ok So I'm using an LPC1679 board , I'm now trying to initialize a UART3 interrupt. I plan to use an RBR interrupt to generate and interrupt once 4 characters have been entered into tera terminal. But I'm having trouble finding the U3IER type definitions in the library. Also , once the interrupt is generated , I would want to compare the string of characters that I have received before I do anything.

So I probably need maybe an example on where to find the type definitions or a sample code on how a UART3 interrupt is initialized.

Thanks.
0 件の賞賛
返信
1 返信

812件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Superfred on Fri Apr 10 07:23:02 MST 2015
Hello,

see post #9 in this thread for an UART example:
http://www.lpcware.com/content/forum/adc-lpc1769-please-help

Fred
0 件の賞賛
返信