Unexpected DMA Behaviour with LPC1778 Two

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unexpected DMA Behaviour with LPC1778 Two

484件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Jan 14 22:13:31 MST 2013
[FONT=Tahoma][SIZE=1]I'm using LPCXpresso 4.3 to debug (because I am not convinced of v5 stability yet) on WinXP Prof SP3 (32 bit)
LPC1778 Custom PCB

I forgot to set the EnableDMA bit in the FIFO register when I set up my uart (Uart0)
Then I setup the RX DMA channel as if I had.

The surprising thing is that the RX DMA is working as expected -- i.e. received characters can be seen in the DMA
buffer.

Can anyone explain this or othwerwise shed light on the issue.

See also my thread "Unexpected DMA Behaviour with LPC1778".

Mike
[/SIZE][/FONT]
0 件の賞賛
返信
0 返答(返信)