Unable to install

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to install

2,740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by c0dehunter on Tue Sep 11 02:34:47 MST 2012
I am unable to install LPCXpresso (same goes for Red Suite) on 64bit Ubuntu 12.04. I have 32bit support libraries. I am a linux guy so I am pretty sure the configuration is alright as far as the OS is concerned.

If I try to double click the installation nothing happens.

If I run the installer from terminal, I get these (InstallJammer) error:
c0dehunter@mintBox ~/Downloads $ sudo ./Installer_LPCXpresso_4.2.3_255_Linux-x86 
[sudo] password for c0dehunter: 

invalid command name "bind"
    while executing
"::unknown bind Text <Tab>"
    ("uplevel" body line 1)
    invoked from within
"uplevel 1 $next $args"
    (procedure "::obj::Unknown" line 3)
    invoked from within
"bind Text <Tab>"
    (procedure "::InstallJammer::InitializeGui" line 19)
    invoked from within
"::InstallJammer::InitializeGui "
    (procedure "::InstallJammer::InitInstall" line 68)
    invoked from within
"::InstallJammer::InitInstall"
    (file "/installkitvfs/main.tcl" line 36228)


If I try to run the installer from terminal, but with "--mode console" flag:
This will install LPCXpresso on your computer.  Continue? [n/Y] Y


Where do you want to install LPCXpresso? [/usr/local/lpcxpresso_4.2.3_255] 

Installing LPCXpresso...
Error in action ExecuteAction

Error in action InstallSelectedFiles

couldn't execute "/tmp/ijtmp_5A0F6295-D9B0-C0B3-49BF-0954047E4DE0/installkit": permission denied
    while executing
"open $cmd"
    (procedure "::InstallJammer::actions::InstallSelectedFiles" line 131)
    invoked from within
"::InstallJammer::actions::$component $self"
    while executing
"::obj::classes::Action::Method_execute ::obj::classes::Action Action1"
    ("uplevel" body line 1)
    invoked from within
"uplevel 1 [list $command $classns $obj {*}[lrange $args 2 end]]"
    (procedure "::obj::Unknown" line 11)
    invoked from within
"$obj execute"
    (procedure "::InstallJammer::ExecuteActions" line 85)
    invoked from within
"::InstallJammer::ExecuteActions $action -parent $id -conditions $eval"
    (procedure "::InstallJammer::actions::ExecuteAction" line 35)
    invoked from within
"::InstallJammer::actions::$component $self"
    while executing
"::obj::classes::Action::Method_execute ::obj::classes::Action DF5A8644-E41D-4C27-B8B5-26C5E8BD7102"
    ("uplevel" body line 1)
    invoked from within
"uplevel 1 [list $command $classns $obj {*}[lrange $args 2 end]]"
    (procedure "::obj::Unknown" line 11)
    invoked from within
"$obj execute"
    (procedure "::InstallJammer::ExecuteActions" line 85)
    invoked from within
"::InstallJammer::ExecuteActions Console"
    (procedure "::InstallJammer::InstallMain" line 11)
    invoked from within
"::InstallJammer::InstallMain"
    (procedure "ThemeMain" line 2)
    invoked from within
"ThemeMain "
    invoked from within
"if {![info exists ::InstallJammer]} { ThemeMain }"
    (file "/installkitvfs/main.tcl" line 36318)


I tried reversing tcl from ver. 8.5 to 8.4 - it didn't help. Also, I tried running all of the above commands as sudo and even from su. Also chmodded and chowned, nothing helped.

Does anyone have any other suggestion? If not, who should I contact further about this? I was forced to temporarily reassign 7 developers to another project branch due to this error.
0 Kudos
Reply
4 Replies

2,451 Views
graygirling
NXP Employee
NXP Employee

The installation README for LPCXpresso should include information about which packages are needed when running LPCXpresso on a 64-bit installation.  Basically the installer requires all the 32-bit libraries needed for GTK2/installjammer.  Have you tried installing them?

0 Kudos
Reply

2,451 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 11 06:08:45 MST 2012
Ubuntu is a supported platform. So, yes, it works.
0 Kudos
Reply

2,451 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by c0dehunter on Tue Sep 11 05:22:58 MST 2012
You are right, it is not Ubuntu, it is Linux Mint.

I need to know if LPCXpresso runs perfectly alright on Ubuntu though? If yes then I can be sure it's something distribution related.

Thanks
0 Kudos
Reply

2,451 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 11 03:17:50 MST 2012
Are you *sure* that is really Ubuntu? It looks like Mint (which is *not* Ubuntu, despite what they may say).

Edit: I see you have posted the same question on the Linux Mint forum. So it is not Ubuntu....
0 Kudos
Reply