Unable to enter debug mode in LPCXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to enter debug mode in LPCXpresso

734 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by isotot on Tue Aug 18 22:47:08 MST 2015
Hi,
I am using a LPC11C14 with a LPCXpresso baseboard along with LPCXpresso IDE.
When I try to debug my code on a standalone XPresso board, everything works fine.
However, when I plug in the LPC11C14 onto the baseboard, i am unable to enter the debug mode.

Please let me know if there are any jumper settings on the Xpresso baseboard i need to take care of , to enable the debug mode.

Thanks,
0 项奖励
回复
1 回复

713 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 19 03:44:57 MST 2015
Usual problem is that you are not providing separate power to the baseboard. Simply connecting the LPCXpresso target board via its debug USB connector is not sufficient.

For more information, read the documentation available from the Embedded Artists website:

[list]
  [*]http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php
[/list]

If that doesn't help, then post details of how your baseboard is configured, plus the LPCxpresso IDE debug log from a failed connection...

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/debug-log
[/list]

Regards,
LPCXpresso Support
0 项奖励
回复