USB finit() Error in LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB finit() Error in LPC1788

911件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by research on Wed Feb 03 04:25:48 MST 2016
Hi,

We are using 1788. we are starting to work USB. in First Step, finit(U0:), it fails and return Error "1"  (IO Error. IO/driver initialization failed, or there is no media, or media initialization failed. )

anybody can help?



0 件の賞賛
返信
2 返答(返信)

894件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by research on Sun Feb 14 23:21:54 MST 2016
Hi,

thank you for your reply

we are using lpc177x.lpc178x.cmsis.driver.library. We are also using TCPIP. It is works well.
Regards
Research
0 件の賞賛
返信

894件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Feb 04 21:47:01 MST 2016
Hi research,
Which code base are you using? Are you using LPCopen?
0 件の賞賛
返信