USB Suspend / Resume for LPC1343 from USBHID example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Suspend / Resume for LPC1343 from USBHID example code

852件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wsyuen on Thu Jul 28 21:10:14 MST 2011
Dear All,

I used the USBHID example code to implement a USB keyboard.
The keyboard function is work.
However, when the computer is suspended, it cannot wakeup by the keyboard anymore.
I saw there are functions like USB Suspend & USB Resume in the example, but how to modify them so that it supports this function?
Thank you.
0 件の賞賛
返信
1 返信

827件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by danhauck on Mon Aug 08 03:02:30 MST 2011
Hi, have you solved the problem? I have the same one.
0 件の賞賛
返信