USB Host Hang errata

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Host Hang errata

769 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sarmitage on Mon Jul 18 13:55:46 MST 2011
I am considering using a LPC1768 and I've noticed that many (if not all) LPC's with USB OTG have an errata regarding a problem that causes the chip to hang in USB host mode if a dribble bit is encountered.

The errata implies that this happens if there is a hub between the LPC and the device.  Am I immune from this problem if there is no hub?

Do the currently shipping revisions of the LPC1768 (or any LPC17xx) have this problem fixed?
0 Kudos
Reply
1 Reply

740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Wed Jul 20 11:21:46 MST 2011
Hello sarmitage,

Sorry, no solution yet ... otherwise the work-around could be: not to use a hub ...
0 Kudos
Reply