USB Callback

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Callback

761件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nasib on Sat Feb 16 01:39:18 MST 2013
Hi all!

I have developed a complete USB aplication in my PC, also i have programed de lpcxpresso11U14 to receive data from PC. About this there is no problem.

But when i want to write a callback from the device to the PC i always write 000000, and i don't know why, because i am writing ok in the buffer and i test it.

Anyone know if i could do something special to achieve it.

Thank you very much!
0 件の賞賛
返信
1 返信

750件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cwpjr on Mon Feb 18 15:12:00 MST 2013
If you have any links that were helpful in learning how to develop the PC side USB app I'd appreciated if you would share.

Thanks, Clyde
0 件の賞賛
返信