USB Bootloader with USB Memory Stick without a PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Bootloader with USB Memory Stick without a PC

586 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Wed Dec 12 01:06:52 MST 2012
Hi everybody! Is there the possibility with LPC1768 to load firmware throught an USB  Memory Stick without a PC? I think that I have to implement USB MAss Storage Class in Bootloader  Mode. So at reset if a GPIO is in a particular state, I enter Bootloader  mode, I read the Memory stick throught File system (USB Host lite) and  if there is a valid .bin file I write it into Flash. All without a PC.  Freescale Kinetis has this feature. Is it possible with NXP LPC1768? Is there an application note for it?
Thank you very much
0 Kudos
Reply
0 Replies