UARTDMA example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UARTDMA example

731件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by strider51 on Mon Sep 09 18:47:47 MST 2013

Hi,
  I am using the MCB1700 example project for the UARTDMA example. I compiled it to in the LPCxpresso Code_Red environment for the 1769 LPCxpresso board. I was able to download it and run it but only part of it works. I can get the first part transmitting from the DMA but I cannot  receive any characters. It sits there in the loop waiting for the flag to say it has transmitted. has anybody had success with this example code? are there any problems with using the example on the 1769 board. It says it is for the lpc1768. any help would be appreciated. thands
0 件の賞賛
返信
1 返信

715件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by strider51 on Tue Sep 10 04:34:23 MST 2013
Hi,
   My previous post I had an error. I did not mean I was waiting for the transmit flag but the flag to say the DMA received the incoming data. thanks.
0 件の賞賛
返信