Timer 2 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timer 2 problem

703件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ramesh@spatika on Mon Aug 30 23:41:17 MST 2010
Hi,
Last week i was trying to initialise timer 2 in lpc 1768 for using as a counter.

But, unfortunately as soon as the program is started the programs stops in a hard fault handler()


kindly clarify me if someone has any solution for the same.
0 件の賞賛
返信
1 返信

675件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Aug 31 00:07:56 MST 2010
For information on how to go about debugging a hard fault, please see:

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/52

You might also want to take a look at the "RDB1768cmsis_timers" example (supplied with LPCXpresso 3.4.6, or downloadable from http://support.code-red-tech.com/CodeRedWiki/RDB1768V2Support). This example sets up the 4 timers to be found in the LPC1768 MCU, and flashes the  LEDs based on when the timers trigger interrupts - one LED per timer  interrupt. Note though that the LED related code in this example is for Code Red's RDB1768 board, and will not work directly on the LPCXpresso1768 board. However the timer code may give you useful pointers for your own code.

Regards,
CodeRedSupport
0 件の賞賛
返信