Target reports errors while debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Target reports errors while debugging

1,021 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Wed Nov 30 23:53:38 MST 2011
I am using LPCXpresso LPC1114 my target is reporting some error while debugging error message is-
Reason-
15:Target errorfrom set break/watch
What could be the reason?:(
0 项奖励
回复
2 回复数

934 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Thu Dec 01 01:16:39 MST 2011
Breakpoints are limited. LPC1769 is limited to 6 breakpoints at the same time. LPC1114 limit is probably less than 6.

Angelo
0 项奖励
回复

934 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Dec 01 00:50:09 MST 2011
Could be helpful if you post your Build log:

http://support.code-red-tech.com/CodeRedWiki/BuildConsole

Could be a reset problem, did you try to enable vector catch?
0 项奖励
回复