Target errors from Commit Flash write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Target errors from Commit Flash write

795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dexter on Fri Sep 10 04:48:42 MST 2010
Hi,
I have a problem. I’m using the LPCXpresso Board Target LPC1114. My project has worked before but now when a run debug I get an error:

Target reported errors
Reason:
15: Target errors from Commit Flash write
Flash erase or write operation aborted.

Please help
Regards,
dexter
0 项奖励
回复
2 回复数

778 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dexter on Sun Sep 12 22:35:44 MST 2010
Thanks for help, my board is working again. :)
dexter
0 项奖励
回复

778 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Sep 10 05:31:14 MST 2010
Most likely reason is that you have managed to program some code into the flash that has destabilized the clock. Take a look at the following faq for ways of getting out of this...

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/44

Regards,
CodeRedSupport
0 项奖励
回复