SysTick.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SysTick.h

660件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by deBoogle on Mon Feb 21 14:44:27 MST 2011
Hi guys,

Just a quick question. I was looking through all the header files for systick functions and found the following in the systick header:

/* Exported functions ------------------------------------------------------- */
void SysTick_Handler(void);
void delaySysTick(DWORD tick);
void SysTick_CLKSourceConfig(DWORD SysTick_CLKSource);
void SysTick_SetReload(DWORD Reload);
void SysTick_CounterCmd(DWORD SysTick_Counter);
void SysTick_ITConfig(FunctionalState NewState);
DWORD SysTick_GetCounter(void);
FlagStatus SysTick_GetFlagStatus(BYTE SysTick_FLAG);


What are these functions for?

I tried using the flagstatus function and it didn't work!

I have found a way around this using the examples provided, and also written some code to detect flag status like the following:

#define count_flag (1<<16)
flag_status = SysTick-> & count_flag;

Just wondred what those functions in the header were for?

Also, (I know big post syndrome!),

Where can I find the defs / declrations for this function which is in the example, I can't see it!

__INLINE static void systick_delay (uint32_t delayTicks)

Why __INLINE??

thanks

deBoogle
0 件の賞賛
返信
0 返答(返信)