Spam attacks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spam attacks

1,128件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jan 20 07:17:55 MST 2011
Hello NXP,

Unwanted ads are flooding the forum, and even worse without pictures of women. :D

I wonder if it automatically or some users are unhappy with the service.

Why the administrators do not erase these ads immediately?

Thank you.
0 件の賞賛
返信
4 返答(返信)

1,122件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Jan 20 13:27:24 MST 2011
Hi Luis,

We delete the SPAM everyday but new spam is soon posted. It is affecting numerous forums using the same software that we are using. We are investigating ways to reduce SPAM. Please be patient...

Thank you,
-NXP
0 件の賞賛
返信

1,122件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Thu Jan 20 09:46:59 MST 2011

Quote: KTownsend
Depending on the version of vbulletin, the reCAPTCHA data can be bypassed automatically.  Definately annoying, though.


Really annoying...
0 件の賞賛
返信

1,122件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Thu Jan 20 09:11:30 MST 2011

Quote: renan
And to register here, there is reCAPTCHA, but I guess this is not working anymore... :confused:



Depending on the version of vbulletin, the reCAPTCHA data can be bypassed automatically.  Definately annoying, though.
0 件の賞賛
返信

1,122件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Thu Jan 20 08:23:01 MST 2011

Quote: Luis Digital
Hello NXP,

Unwanted ads are flooding the forum, and even worse without pictures of women. :D

I wonder if it automatically or some users are unhappy with the service.

Why the administrators do not erase these ads immediately?

Thank you.



And to register here, there is reCAPTCHA, but I guess this is not working anymore... :confused:
0 件の賞賛
返信