Show Peripherals+ with Segger J-link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Show Peripherals+ with Segger J-link

722 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LVL on Wed May 07 06:30:32 MST 2014
Is it possible to show the Peripherals in the Peripherals+ window with J-link?
I like the LPC-Link 2 a lot, but it is far slower than J-link.
If this would be possible, I don't think I have anything bad to say about LPCXpresso. :)

Thank you in advance for answering my question. (I couldn't find one after a LOT of searching)
0 Kudos
Reply
2 Replies

660 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Petervg on Sat Nov 08 05:51:16 MST 2014
Will this issue be solved in the near future? I really would like to use the J-link for it's speed because the link2 is way too slow and has issues when connected together with the labtool I use as logic analyzer. Debugging support has gone downhill imo since NXP has acquired code red and cancelled the red probe...

I found a website (http://gnuarmeclipse.livius.net/blog/peripheral-registers/) where a solution is available to support the registers view in eclipse using the J-link, but for some reason I cannot install the packs they are talking about. The menu options just aren't visible in my version of lpcxpresso. Guess the page is for a ' vanilla'  eclipse environment...




0 Kudos
Reply

660 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed May 07 06:34:00 MST 2014
No. J-Link is not compatible with the Peripherals view.
0 Kudos
Reply