Serial port CDC WinCE 6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial port CDC WinCE 6

1,221 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Wed Jul 20 13:15:37 MST 2011
Hello,

What is necessary to recognize the device USB serial CDC in WinCE 6?

I use the FTDI chip, but comes with a driver and a .inf file.

Because the chip LPC134x uses a generic implementation not need a driver, only the .inf file to configure the Registry.

Any guidance is appreciated.

Thanks.
0 项奖励
回复
3 回复数

1,117 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jul 21 14:52:31 MST 2011
The funny thing is that reestablished the original configuration, and I realized that it is installed and configured a serial port, just as does the Microsoft website. Apparently the port is for internal use/debugging.

But changing the PID and VID, solves nothing.

I tried other methods, such as FTDI does:
[HKEY_LOCAL_MACHINE\Drivers\USB\LoadClients]
[VID_PID]
[Default]
[Default]
[USBSER_Class]
REG_SZ "Dll"="serialusbfn.dll"


VID and PID in Decimal.

I give up, and I leave the revenge to another.

I am using a laptop: WinCE 7" $80 - $100 (eBay).
0 项奖励
回复

1,117 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jul 21 06:32:41 MST 2011
I'm trying (unsuccessfully) some indication from Microsoft, but it always appears the message:
This device is not found in the supported USB device table.


I'm changing the PID and VID correctly.

Also a window appears asking: "Driver Name", does not really know what to do. I had never used WinCE before.

If I have success I will report.

Thank you.
0 项奖励
回复

1,117 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Thu Jul 21 00:39:50 MST 2011
Hi Luis,
Don't have the WinCE 6 drivers for the LPC13xx VCOM, but as guidance I attached the .inf files for Win XP and Win 7.
Perhaps with looking at the FTDI driver and Win XP/7 driver for LPC1300 you'll be able to make a .inf-file for WinCE 6.

If it works, could you please post it on the forum?

Kind regards,
0 项奖励
回复