Serial Wire Debug Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial Wire Debug Interface

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 29 05:36:30 MST 2010
Just trying to reduce the size of my new LPC1768 Board and checked my SWD-Connector (SWDCLK, SWDIO, SWO, GND).

My Scope doesn't show any activity at SWO-Pin so I disconnected this wire and LPCXpresso seems to work without problems.

User manual describes SDO as something optional:

"SWO Output Serial Wire Output. The SWO pin optionally provides data from the ITM and/or the ETM for an external debug tool to evaluate."

Don't understand that and don't know if SDO is used by LPCXpresso at all.

Does anyone know if SDO is optional or if I lose LPCXpresso functions after reducing my Debug Interface to SWDCLK, SWDIO and GND ?
0 项奖励
回复
2 回复数

1,468 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 29 06:03:36 MST 2010
Thanks for your quick response.

- Zero
0 项奖励
回复

1,468 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 29 05:44:33 MST 2010
SWO is not used by LPCXpresso. However, Red Suite uses this for the Red Trace feature
0 项奖励
回复