Serial Wire Debug Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial Wire Debug Interface

1,538 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 29 05:36:30 MST 2010
Just trying to reduce the size of my new LPC1768 Board and checked my SWD-Connector (SWDCLK, SWDIO, SWO, GND).

My Scope doesn't show any activity at SWO-Pin so I disconnected this wire and LPCXpresso seems to work without problems.

User manual describes SDO as something optional:

"SWO Output Serial Wire Output. The SWO pin optionally provides data from the ITM and/or the ETM for an external debug tool to evaluate."

Don't understand that and don't know if SDO is used by LPCXpresso at all.

Does anyone know if SDO is optional or if I lose LPCXpresso functions after reducing my Debug Interface to SWDCLK, SWDIO and GND ?
0 Kudos
Reply
2 Replies

1,453 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 29 06:03:36 MST 2010
Thanks for your quick response.

- Zero
0 Kudos
Reply

1,453 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 29 05:44:33 MST 2010
SWO is not used by LPCXpresso. However, Red Suite uses this for the Red Trace feature
0 Kudos
Reply