Selecting project in project tree jumps to another project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Selecting project in project tree jumps to another project

680 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lu_bo on Fri Jun 19 12:35:59 MST 2015
Hi, guys!

I have an LPC workspace with three projects:

- lpc_board_nxp_lpcxpresso_1343
- lpc_chip_13xx
- Myproject

I'm using LPCXpresso v7.8.0. Myproject uses printf through UART0. Myproject is linked with the other two projects. If I get an error in some of those projects (the board or the chip), when I select Myproject in the project tree the selection automatically jumps to the project with the error and opens the file with the problem. This is very annoying and I believe it's some magical Eclipse's feature that I need to turn off.

Thanks in advance,
L. B.
0 项奖励
回复
2 回复数

660 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Jun 19 13:26:49 MST 2015

Quote: lu_bo
This is very annoying and I believe it's some magical Eclipse's feature that I need to turn off.



That's no feature and usually it's enough to restart LPCXpresso...
0 项奖励
回复

660 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Jun 19 13:10:51 MST 2015
After 7 years of using eclipse, I have never seen it do that! If it is a workspace setting, try opening the preferences and Restore Defaults. If not, try exporting you projects, create a new workspace and import them.
0 项奖励
回复