Secret enmity between Debug buttons and Restart button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secret enmity between Debug buttons and Restart button

1,287 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Sun Nov 11 10:23:01 MST 2012
I'm able to move Restart button in Toolbar (Develop Perspective) from the right side to the other Debug buttons at the left side of Toolbar (LPCXpresso V5, Win7Pro,Theme:Windows7).

So far, so good :)

Closing LPCXpresso and opening it again moves it back to it's default position :eek:

Is that an (Eclipse-) bug / feature or is that a secret button enmity :confused:

Perhaps it's possible to move Restart button beside debug buttons in next release?
0 Kudos
Reply
4 Replies

1,275 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Wed Nov 14 07:39:32 MST 2012
Thanks :)
0 Kudos
Reply

1,275 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Nov 14 05:17:28 MST 2012
We'll take a look at whether there is anything we can do regarding the positioning of restart.

Regards,
CodeRedSupport
0 Kudos
Reply

1,275 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Nov 13 08:41:14 MST 2012

Quote: kayoda
Closing LPCXpresso and opening it again moves it back to it's default position :eek:



Same problem here with Win8Pro :o
0 Kudos
Reply

1,275 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Sun Nov 11 13:03:22 MST 2012
Same happens with the key bindings :D
0 Kudos
Reply