Secret enmity between Debug buttons and Restart button

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secret enmity between Debug buttons and Restart button

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Sun Nov 11 10:23:01 MST 2012
I'm able to move Restart button in Toolbar (Develop Perspective) from the right side to the other Debug buttons at the left side of Toolbar (LPCXpresso V5, Win7Pro,Theme:Windows7).

So far, so good :)

Closing LPCXpresso and opening it again moves it back to it's default position :eek:

Is that an (Eclipse-) bug / feature or is that a secret button enmity :confused:

Perhaps it's possible to move Restart button beside debug buttons in next release?
0 件の賞賛
返信
4 返答(返信)

1,284件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Wed Nov 14 07:39:32 MST 2012
Thanks :)
0 件の賞賛
返信

1,284件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Nov 14 05:17:28 MST 2012
We'll take a look at whether there is anything we can do regarding the positioning of restart.

Regards,
CodeRedSupport
0 件の賞賛
返信

1,284件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Nov 13 08:41:14 MST 2012

Quote: kayoda
Closing LPCXpresso and opening it again moves it back to it's default position :eek:



Same problem here with Win8Pro :o
0 件の賞賛
返信

1,284件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Sun Nov 11 13:03:22 MST 2012
Same happens with the key bindings :D
0 件の賞賛
返信