Saving Data on M0+ ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Saving Data on M0+ ??

1,167 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by klikla on Thu Nov 26 10:03:52 MST 2015
Hi everyone,
i want to save some data i get from  the thermometer (the board is not connected to the PC).
After the routine i want to connect the board to my PC and start the debug and read the values?
Is this possible or not ?

Im using the LPC82 Board.

0 项奖励
回复
3 回复数

1,153 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by klikla on Mon Nov 30 02:07:19 MST 2015
Thank You :bigsmile:
This helps me much
0 项奖励
回复

1,153 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Nov 26 18:05:48 MST 2015
And make sure that you do not loose power when changing from monitoring mode to debug mode.
[Because ram based variables will be lost and peripherals will be reset -- obviously.]

Mike
0 项奖励
回复

1,153 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Nov 26 10:26:16 MST 2015

Quote: klikla
Is this possible or not ?



Yes, use 'Attach only'  :O

https://www.lpcware.com/content/faq/lpcxpresso/debugging-running-system
0 项奖励
回复