SWIM graphics library for LPCXpresso IDE example project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWIM graphics library for LPCXpresso IDE example project

1,554 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by legato on Thu May 23 20:34:21 MST 2013
Hello guys,

         Do we have here an [COLOR=Red][B]example project for SWIM graphics library[/B][/COLOR] [B][COLOR=Red]for lpcxpresso ide[/COLOR][/B]. If you have there or know anything about it maybe you could hit a comment and a link for it. I want to evaluate and try an example from it. thanks.
0 Kudos
Reply
2 Replies

1,245 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjm on Thu Aug 20 03:45:50 MST 2015
I'm trying to get it work with Olimex MOD-LCD4.3
The example project is based on a Keil eval board.

Finally, build has been succeeded, but the TFT does not work as expected. Prior to supplying details, I'd ask now whether anybody has this Olimex board running with SWIM (or even EMlib, which seems however quite complicated, according to other threads like https://www.lpcware.com/content/forum/hotmcu-lpc1788-dev-board-43-inch-lcd and https://www.lpcware.com/content/forum/driving-controllerless-lcd-43-inch .
0 Kudos
Reply

1,245 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri May 24 00:57:25 MST 2013
There are samples included in  LPC1788 Developer's Kit.

See: http://lpcware.com/content/blog/swim-lesson-1 , http://lpcware.com/content/blog/swim-lesson-2

Also it's included in LPCOpen: http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers
0 Kudos
Reply