SSP problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SSP problem

777 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Sat Jan 29 14:20:22 MST 2011
Hi, i am making a touchscreen project  which is interfaced via spi. But every time i connect it to my lpcxpresso board i can put the code to it (some kind of error occurs). I dont know how jtag works but i kinda need a solution :) (the problem occurs even when CS for the Touch screen stays high).
0 Kudos
Reply
1 Reply

760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jan 29 14:32:45 MST 2011

Quote: bobi-one
...my lpcxpresso board...



...which LPCXpresso :confused:


Quote: bobi-one
...some kind of error occurs...



...which error :confused:


Quote: bobi-one
... interfaced via spi...



...how :confused:


Quote: bobi-one
...dont know how jtag works...



That's obvious :) LPCXpresso is working with SWD.

Did you use a shared SWD PIN ?
0 Kudos
Reply