SPI failure to launch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI failure to launch

889件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by woodchuck on Wed Apr 06 12:28:14 MST 2011
Would anyone know why the following sequence of instructions fails to get any activity out of the SSP of the LPC1114? I've jumped through all the hoops I can think of. Surely vectored interrupts aren't required to output a byte via SPI?!


[PHP]
LPC_SYSCON->PRESETCTRL |= 1;         // SSP0_RST_N set to 1

LPC_SYSCON->SYSAHBCLKCTRL |= (1<<11);   // enable SPI0 clock

LPC_SYSCON->SSP0CLKDIV = 0x01;

LPC_IOCON->PIO0_8 &= ~0x07;
LPC_IOCON->PIO0_8 |= 1;                     // config MISO

LPC_IOCON->PIO0_9 &= ~0x07;
LPC_IOCON->PIO0_9 |= 1;                          // config MOSI

LPC_IOCON->SCK_LOC = 0x01;               // select SCK
LPC_IOCON->PIO2_11 = 0x01;                   //  as p2.11

LPC_IOCON->PIO0_2 &= ~0x07;               // Use SSP
LPC_IOCON->PIO0_2 |= 0x01;                   //  SSEL

LPC_SSP0->CR0 = 0xEF07;              // 8-bit, SPI, CPOL0, CPHA0, 100 KHz

LPC_SSP0->CPSR = 0x2;                  // this is the minumum divisor

LPC_SSP0->CR1 = 4;                        // select master mode

LPC_SSP0->CR1 |= 2;                       // enable SPI

LPC_SSP0->DR = 0x1234;                // write something to tx fifo
[/PHP]
0 件の賞賛
返信
2 返答(返信)

875件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by woodchuck on Wed Apr 06 13:36:06 MST 2011
Right location, wrong state. Thank you very much for catching this!!!

Edit: Program works beautifully. :)
0 件の賞賛
返信

875件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Apr 06 13:11:36 MST 2011

Quote:

LPC_SSP0->CR1 = 4;                        // select master mode



That's wrong :):)

This bit selects slave mode, so it's waiting for a master....
0 件の賞賛
返信