SPI communication - SSP1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI communication - SSP1

733 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eduardo on Mon Jun 14 06:59:48 MST 2010
Dear all,

I'm trying to build a SSP1 driver on my LPC1114 development board, but no success until now.
I'm quite new to this kind of embedded development (i was usually developing just desktop softwares), so that's is a huge work for me.

I'm working with Lib_MCU (that comes with LPC expresso compiler), as you can see on attached files, i've made some modifications that I think it's not correct (I based all the ssp1 functions on ssp0 functions).

Someone knows any link or tip that will help me?

Thanks in advance.
0 Kudos
Reply
1 Reply

721 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri Jun 18 11:29:02 MST 2010
Hi eduardo,
Did you tried one of the example projects which comes with the LPCXPresso?
This example is tested and working fine, so it sould get you started quickly.

Some directions: Quickstart Pan -> Import example project -> ...

If you have a Embedded artists base board, that also comes with quite some neat examples.

Kind regards,
0 Kudos
Reply