SD card detection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD card detection problem

730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ranaya on Sat Nov 03 09:52:42 MST 2012
hello all,

This question is about interfacing an SD memory card with LPC1769 xpresso board. Im using chan's fatfs library.

   When the SD card is connected (to the socket) before power up the board, the disk_initalize() function return an error(1) in debugging mode. Then without removing power I reconnected the SD card to the socket, and disk_init recognized the card. I am using all SPI lines (not card detect), and double checked their connections. What i dd wrng ? luking 4 ur quick replies.
    
Thanx
0 件の賞賛
返信
1 返信

685件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by modestt on Mon Nov 05 03:02:28 MST 2012
If you look for my previous posts I posted working code(tested) 1769 interfaced  with SD card(I vaguely recall it was SSP0).
0 件の賞賛
返信