SCT used as PWM Generator does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCT used as PWM Generator does not work

891 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ucniranjan on Wed Jan 22 04:56:32 MST 2014
Friends,

I am using the LPCXpresso 812 Board with the IDE. I have a simple program, wherein I initialize the SCT as a PWM timer, with 1/3 duty cycle. The SCT spec: 12MHz clock, 16-bit counter, 2 events and interrupt mode. I redirect the SCT output to pin 7. The main function instantiates 
PWM bursts of 20 pulses. When I run the code below, and connect the Logic Analyzer to pin 7, I do not see the PWM pulses. What could be wrong? I feel I am missing somethin in initializing the SCT. I have used the default libraries of LPCXpresso.

Thanks,
Niranjan

/****************************************************************************
Main Function
****************************************************************************/
#ifdef __USE_CMSIS
#include "LPC8xx.h"
#endif

#include "lpc8xx_clkconfig.h"
#include "lpc8xx_gpio.h"


static volatile uint32_t PWMCount = 0;

void SCT_IRQHandler(void)
{
PWMCount--;
if(PWMCount == 0)
{
LPC_SCT->CTRL_L    |= (1 << 2);
}
LPC_SCT->EVFLAG = (1 << 0);
}

void PWM_SCT_Init(void)
{
    LPC_SYSCON->SYSAHBCLKCTRL |= (1 << 8);                 // SCT clock

    LPC_SYSCON -> PRESETCTRL &= ~(0x1<<8);
    LPC_SYSCON -> PRESETCTRL |=  (0x1<<8);

    LPC_SCT->CONFIG |= (1 << 17);                          // Two 16-bit timers, auto limit
    LPC_SCT->CTRL_L |= (SystemCoreClock/12000000-1) << 5;  //  SCT clock = 12 MHz

    LPC_SCT->MATCH[0].L    = 360;                          // match 0 @ 30 usec
    LPC_SCT->MATCHREL[0].L = 360;
    LPC_SCT->MATCH[1].L    = 240;                          // match 1 @ 20 usec
    LPC_SCT->MATCHREL[1].L = 240;

    LPC_SCT->EVENT[0].STATE = 0x00000001;                  // event 0 only happens in state 0
    LPC_SCT->EVENT[0].CTRL  = (0 << 0)  |                  // MATCHSEL[3:0] = related to match 0
                              (1 << 12) |                               // COMBMODE[13:12] = match condition only
                              (1 << 14) |                              // STATELD[14] = STATEV is loaded into state
                              (0 << 15);                              // STATEV[15] = 0

    LPC_SCT->EVENT[1].STATE = 0x00000001;                  // event 1 only happens in state 0
    LPC_SCT->EVENT[1].CTRL  = (1 << 0)  |                  // MATCHSEL[3:0] = related to match 1
                              (1 << 12) |                               // COMBMODE[13:12] = match condition only
                              (1 << 14) |                              // STATELD[14] = STATEV is loaded into state
                              (0 << 15);                              // STATEV[15] = 0

    LPC_SCT->EVEN = (1 << 0);
    NVIC_EnableIRQ(SCT_IRQn);                              // enable SCT interrupt
    NVIC_SetPriority(SysTick_IRQn, 3);   // Give less priority to SysTick_IRQn

}

void Start_PWM(uint32_t pwmcount)
{
PWMCount = pwmcount;
LPC_SCT->CTRL_L    &= ~(1 << 2);                       // unhalt SCT

while(PWMCount)
{
LPC_SCT->OUT[0].CLR = (1 << 0);       // event 0 will set SCT_OUT_0, SETCLR0 = 0
LPC_SCT->OUT[0].SET = (1 << 1);      // event 1 will clear SCT_OUT_0, SETCLR0 = 0
}

}

/* Main Program */

  int main (void) {
  uint32_t regVal;

  SystemCoreClockUpdate();

  /* Config CLKOUT, mostly used for debugging. */
  regVal = LPC_SWM->PINASSIGN8 & ~( 0xFF << 16 );
  LPC_SWM->PINASSIGN8 = regVal | ( 12 << 16 );
  CLKOUT_Setup( CLKOUTCLK_SRC_MAIN_CLK );

  LPC_SWM->PINASSIGN6 = 0x07FFFFFF;                          // SCT OUTP_0 at P0.7
  PWM_SCT_Init();
     
int i1;
  while(1)
  {
  Start_PWM(20);
  for (i1=0; i1<100000; i1++) {  __NOP(); }
  }

}
0 Kudos
Reply
1 Reply

805 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Jan 23 12:06:29 MST 2014
Hi ucniranjan,
I suggest you to have a look into  PWM example with SCT from LPCopen code. See below link.
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc8xx-packages
0 Kudos
Reply