Run the code without debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run the code without debug

1,348件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ngoncalves on Fri Sep 30 06:43:45 MST 2011
Hi,

  Is it possible to download the firmware and run it without using the debug mode ?

  I have the free edition of the LPXpresso and I know about the limitation to 128K, but my firmware is less than 1 K. I should be able to download it and run, but so far I can only download firmware by pressing the debug button.

  Nelson
0 件の賞賛
返信
3 返答(返信)

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 30 09:58:18 MST 2011

Quote: ngoncalves
My guess is that I need to have a project opened, otherwise it does not work.



This tool needs a 'target' information. Therefore it will not work without opened project :)
0 件の賞賛
返信

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ngoncalves on Fri Sep 30 09:41:46 MST 2011

Quote: Zero
'Program Flash' (little chip icon) is what you're looking for :)

Note #1: Running after Program isn't always working, see: http://knowledgebase.nxp.com/showthread.php?t=2422

Note #2: 'Command Line Programming' is described here: http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming?



Thanks. That was the button I had pressed earlier but it gave me an error about memory limits. But now it works.

My guess is that I need to have a project opened, otherwise it does not work.
0 件の賞賛
返信

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 30 08:14:28 MST 2011
'Program Flash' (little chip icon) is what you're looking for :)

Note #1: Running after Program isn't always working, see: http://knowledgebase.nxp.com/showthread.php?t=2422

Note #2: 'Command Line Programming' is described here: http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming?
0 件の賞賛
返信