Return code: 0x86

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Return code: 0x86

1,361件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Feb 17 02:47:39 MST 2015
Dear all: I use LPCXpresso  v7.5.0 [Build 254] [2014-10-31]  connect to LPC_Link with my target.
The second time that I start the debug connect appar this message:

Flash driver "Init" return code: 0x86

and after :

InterruptedException
Timeout waiting for StubMonCapabilities: -interpreter-exec console "mon capabilities"

Timeout waiting for StubMonCapabilities: -interpreter-exec console "mon capabilities"
  at com.crt.dsfdebug.dsf.commands.MIStubCommandBase.getResult(MIStubCommandBase.java:128)
  at com.crt.dsfdebug.dsf.commands.MIStubCommandWrapper.getResult(MIStubCommandWrapper.java:110)
  at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.processMIOutput(AbstractMIControl.java:908)
  at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.run(AbstractMIControl.java:755)

After disconnet and re-connect the LPC_Link, the first time all is ok.

How can I solve this problem ?

Thanks





0 件の賞賛
返信
2 返答(返信)

1,286件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Feb 17 08:12:39 MST 2015
I have solved the problem setting in Debug Configuration -> Debug -> Vector catch = True .
This setting affects how ?
I don't understand how one can be solved the problem . . .

Thanks
0 件の賞賛
返信

1,286件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 17 04:33:32 MST 2015
This sounds like one of the problems described here:
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

0 件の賞賛
返信