Registration on multiple machines?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Registration on multiple machines?

895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPCVictoria on Wed Dec 02 17:37:33 MST 2009
Hi-

I now have a couple of LPCExpresso 1343s (yay).  If I register an LPCXpresson on one machine, am I limited to that machine, or can I move to another machine, or move between machines? 

Thanks,
David
0 件の賞賛
返信
2 返答(返信)

889件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPCVictoria on Fri Dec 04 18:30:36 MST 2009
Thx.

David
0 件の賞賛
返信

889件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Dec 03 17:58:18 MST 2009
Hi David,

To install the LPCXpresso IDE on another machine, you will need to go to that PC and log into www.code-red-tech.com/lpcxpresso with the username and password you received when you first registered to download the LPCXpresso IDE. It is easiest if you use Internet Explorer. Then, after logging in, install and start the LPCXpresso IDE, and complete the activation process.

You should only need to register with your email address once.
The LPCXpresso IDE should be activated on each machine it is installed on.
The LPCXpresso boards do not contain a serial number and are interchangeable.

Thank you,
-NXP Support
0 件の賞賛
返信