Registering??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Registering??

830 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by juyles on Thu Dec 30 08:59:26 MST 2010
I purchased two of the Xpresso modules. Do I need to register them both
with 'Code Red'?

Jules

Original Attachment has been moved to: 1100932_DebugQuitLog.zip

0 Kudos
Reply
1 Reply

771 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Dec 30 09:22:14 MST 2010
You don't (can't) register LPCXpresso hardware with Code Red.

What you do need to do is create yourself an account at:

http://lpcxpresso.code-red-tech.com/LPCXpresso/

This will allow you to download the LPCXpresso IDE to use with your boards. Once you have installed the IDE, you will then need to create an activation code, which involves first of all creating a serial number within the IDE, which is then used to create a corresponding activation code.

For more information on activation, see section 3.3 of

http://ics.nxp.com/support/documents/microcontrollers/pdf/lpcxpresso.getting.started.pdf

Regards,
CodeRedSupport
0 Kudos
Reply