Regarding lpc1788 CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding lpc1788 CAN

695 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by badri89 on Fri Apr 05 04:50:02 MST 2013
Hi all,

I am thinking of using CAN of lpc1788 which is used in my board.

I got confused regarding a few points:

1. Is the isolator is inbuilt in lpc1788, so that I can directly take out CANH,CANL without any isolator IC?

2. What cables should be used for CAN communication.Can I use any cable for CAN? 
c
And also please do some pointers for beginners in CAN.

Thanks!
0 Kudos
Reply
1 Reply

674 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tha on Fri Apr 05 15:13:52 MST 2013
There is a nice CAN primer from the MCB1700.

http://www.keil.com/download/files/canprimer_v2.pdf
0 Kudos
Reply