Regarding LPCXpresso IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding LPCXpresso IDE?

701 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharatelectro on Wed Jun 29 09:50:42 MST 2011
Can I use LPCXpresso IDE for hardware other than LPC. I am currently working on a project which has ARM 968 processor,  which has 32 Kbytes of ROM and 32 Kbyte RAM. I want to port the FREERtos, can I use this IDE to do so, If not what are the alternatives to create a image specific to the processor. I want to first port the FREERtos and then build application on it,
0 Kudos
Reply
2 Replies

693 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akhilpo on Fri Jul 08 10:56:12 MST 2011
Can I use LPC Link with an another IDE other than LPCXpresso?
0 Kudos
Reply

693 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri Jul 08 05:41:10 MST 2011
Currently supported families for LPCXpresso are LPC1100/LPC1200/LPC1300/LPC1700/LPC1800 and LPC4300. Also the LPC2109/LPC2134/LPC2142/LPC2362/LPC2929/LPC3130/LPC3250 parts are supported.
  For all these targets you can use the LPCLink, provided that you have proper pins available on your custom board.
  Since the LPC2929 with the ARM968 core is supported, you can use LPCXpresso for a FreeRTOS port.
0 Kudos
Reply