Redlib source code available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redlib source code available?

1,940 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert hulsebos on Wed Feb 05 14:01:46 MST 2014
Is the source code of the Redlib run-time library available to the public? If so, where can I find it?
0 Kudos
Reply
1 Reply

1,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 06 01:31:51 MST 2014
No, Redlib sources are not available.

Links to the source for the open source components used within LPCXpresso, including Newlib, can be found at:

http://www.lpcware.com/lpcxpresso/downloads/source

Regards,
LPCXpresso Support
0 Kudos
Reply