Redlib in special memory section

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redlib in special memory section

788件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpresso_1769 on Tue Jun 04 08:08:01 MST 2013
Hi there,
I'm currently working with Redsuite 4.2.2 and a LPC1768...

I have also included the Redlib.

My question is now, is it possible to link all functions which are included from the redlib into a special memory section? I thought at the section attribute and a spezial linkerscript?!  :confused:

Is that possible?
Thanks in advance!

Oli
0 件の賞賛
返信
2 返答(返信)

777件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Jun 05 04:32:33 MST 2013
Why do you want to do this?

All code will be placed in the .text section, initialized data in the .data section and uninitialized data in the .bss section. Depending on how code-red compiled their libraries, they may have placed each function into its own section (i.e. .text_function_name) - you would have to look in the link map to find out.

So, you would need to create a linker script that assigns EVERY section to a specific memory region. You would have to update this every time you added/removed a function. A lot of work.

So, again, why do you want to do this?
0 件の賞賛
返信

777件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpresso_1769 on Wed Jun 05 04:10:16 MST 2013
Nobody an idea?!
0 件の賞賛
返信