Redirecting console output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redirecting console output

1,097件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Underling on Fri Jan 20 05:42:13 MST 2012
Hi all,

I'd like to dump the console output produced by my target (using semihosting) to a file.

If I use fprintf() to log the data directly to a file, the data appears not to be committed until the file is closed. I've tried repeated opening/closing of a log file on the host machine, and it's very slow. Also, it's useful to see the data on the screen as it appears.

So, is there a simple way to copy or redirect console output to a file, other than copy and paste?

Thanks!
0 件の賞賛
返信
3 返答(返信)

1,080件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Underling on Wed Jan 25 08:40:02 MST 2012
OK, thanks for your help.
0 件の賞賛
返信

1,080件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun Jan 22 05:42:06 MST 2012
I am afraid that there is currently no way of automatically logging the output in the console view out to file, other than copy'n'pasting it.

With regards to the speed of fprintf output, I suggest you take a look at this FAQ:

http://support.code-red-tech.com/CodeRedWiki/WhatIsSemiHosting


Regards,
CodeRedSupport
0 件の賞賛
返信

1,080件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dragilla on Fri Jan 20 05:50:18 MST 2012
Don't know about redirecting console, but you can try using f_sync instead of closing and opening the file. It's there just for that.
0 件の賞賛
返信