RedProbe+ alternative

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RedProbe+ alternative

1,454 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrep4 on Wed Jun 04 01:44:31 MST 2014
Hi,

I would like to buy a RedProbe+, but it does not seem to be available anywhere. I would like to use it for profiling my LPC SW. Can anybody recommend an alternative (not LPC-Link, because it will not support profiling)?
0 Kudos
Reply
4 Replies

1,442 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 15 02:04:53 MST 2014
A small number of Red Probe+ units have been tracked down. These can be obtained from Embedded Artists (http://www.embeddedartists.com) on a first come, first served, and no support / no warranty basis. To enquire about remaining Red Probe+ availability, you can contact Embedded Artists via
[list]
  [*]http://www.embeddedartists.com/contact
[/list]

NOTES:
[list=1]
  [*]These are the last Red Probe+ units that will be available.
  [*]We would recommend that such purchases are only considered by customers who are already familiar with the product.
  [*]Red Probe+ is a discontinued Code Red Technologies debug probe, and is no longer being developed or sold by NXP. Although the LPCXpresso IDE will for the moment continue to support the use of Red Probe+ at the current level, no new functionality or new NXP MCU support is planned for Red Probe+.
[/list]

Regards,
LPCXpresso Support
0 Kudos
Reply

1,442 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by afinezzo1968 on Sun Jun 22 08:02:36 MST 2014
Hi, I'm in the same situation. I've found the order code in the Mouser web site but it still unavailable. So I'm understanding why I was unable to find it.
It seems the only one that provides support for Serial Wire Viewer (SWV) tools, for profiling.
If anybody find where to buy a RED Probe+ please make a whistle!!!!
It is known to be really a professional JTAG probe
Many thanks in advance

Alessandro
0 Kudos
Reply

1,442 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrep4 on Thu Jun 19 12:26:32 MST 2014
Hi,

Is there any update on the Red Probe+ availability?

Best regards,
André
0 Kudos
Reply

1,442 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jun 05 00:44:49 MST 2014
Support for profiling using LPC-Link2 is in development, but is unfortunately still some way from being released. I will investigate what the current situation is with Red Probe+ availability.

Regards,
LPCXpresso Support
0 Kudos
Reply